I am a first time user of the TI Chipcon products and am trying to use the CC1101_CC1190EM 869MHz reference design to layout a "daughter board (DB)" that is to communicate with a "mother board (MB)" via Asynchronous Serial operation. An additional requirement is that the DB interface with the SmartRF development board (via 4-wire SPI). The ref design uses GDO0 and GDO2 to set two of the CC1190 control signals (PA_EN & LNA_EN) while the third control pin (HGM) can be hardwired to GND/VDD. The CC1101 part spec recommends using GDO0 and GDO2 for asynchronous serial operation. Other than using an external MCU, is there a way for the GDOx lines to be used to: 1) use asynch serial comm, 2) control the CC1190 and 3) interface with SmartRF ? Any suggestions/recommendations would be appreciated. Dave