This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm tryig to debug the prog. RF_Toggle_LED_Demo.c which is included in slaa465b.zip (SLAA465 - CC430 RF Examples) via the simulator of IAR for MSP430 ver.5.501.
When I run the frog. step by step I get stack in the command SetVCore(2);
If I break the simulator it goes to the commands :
while ((PMMIFG & SVSMLDLYIFG) == 0); // Wait until SVM low side is settled
remarak this command transfer to :
while ((PMMIFG & SVSMLDLYIFG) == 0); // wait for lowside delay flags
emarak this command transfer to :
while ((PMMIFG & SVSMHDLYIFG) == 0); // Wait until SVM highside is settled
After remarking those lines in hal_pmm.c file the simulator get stack in the folloing line which is InitRadio(); command.
What is the reason for this ? What can I do in order to simulate the program ?
BR
Yaniv