This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC Debugger interface problem with IAR EW8051-ver7.51A

Hi Gentlemen,

I am facing problem with ccdebugger during  entering debug mode. I am using IAR EW8051 ver 7.51A network based license. The warning message  pop on my screen is  : "Target Selection"  Note: A target can not be slected when used in another debus session or in another application.

I have gone through the another posts in TIe2e and applied all the solutions like update patches and all but problem is still there.

In order to cross verify CCDebugger I have have installed same IAR EW8051on another machine and used the same debugger and it is working fine there. As i have to work on my machine i need to make it work here.  Here I am not sure about problem, whether it is with IAR or CCDebugger.

So could you help me out to get rid of this problem.

Thanks