This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

example code for simple remote switch application less then 4k code size ?

Hello Dears,

I have a problem compiling the example code packet named SWRC133.
Due to my information, that is the code, which is preprogrammes on the CC1110DK-Mini-868.
This is the hardware, which is available for me.
Before compiling the code, following error appears (I have the 4k kickstart IAR Workbench Version 8.20.1):

Error[Og008]: Code size limit exceeded (4096 code bytes) for this version of the compiler.

The message is self-explanatory, of course, but I'm asking me, if it's possible to build up a very simple remote switch
based on the code example, which needs less then 4k code size ?

I'm not an expert in Microcontroller-Programming, so I just want to change the code a little bit, to build up my application.

Can anyone help me out, to find a code example ?
Or do I have to find out, what is an open-source alternative to the IAR Workbench ?

Thank you a lot in advance,

Michael