This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF7970A EVM + Android data transfer

Other Parts Discussed in Thread: TRF7970A

Is it possible to connect Android to TRF7970A EVM so that the module can be controlled from the Android? Module should be able to poll for tags, detect them, and send a write/read request to Android (i.e tag data ready to be written)? This should be controllable from Android like in USB controlled GUI in Windows. Futhermore, is this possible with NFC p2p or does the module have to be controlled through USB remote host?

Also is it possible to achieve mentioned control through USB without cp210x drivers?