This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem about ad sample in cc2530

Other Parts Discussed in Thread: CC2530

hi,

I set 1ms timer in cc2530, i read ad smaple value in 1ms timer interrupt and then start adc conversion, but this influence zigbee communication.If I do not start adc conversion, 1ms timer  work good and zigbee communication is ok , I think adc don't   take cpu source ,but timer interrupt do.I don't know why this happend,Some code are below:

HAL_ISR_FUNCTION( D_Time4_Interrupt, T4_VECTOR)

{

     T4IF=0;
     T4CTL=0xd9;

     if(ADCCON1 & 0x80)

    {

         ####; //read ad sample

    }

    ADCCON3=0Xa6; // if i add this instruction ,zigbee communication is not ok, but if i delete it ,communication is ok

}