This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About CC1125 TRX control algrithm?

Other Parts Discussed in Thread: CC1125

Hi

When we disconnect TRX pin, CC1125 still working normally.
1.The TRX pin how to work?
2.CC1125 circuit must be connect TRX pin or not? 

Eric

 

  • The TRX pin is pulled to ground in TX and is open in RX.

    The following is true if the reference design is used and no other adjustments are due except for cutting the TRX line.

    For RX not connecting the TRX pin will have minimal impact on performance since the source impedance for the LNA will be the same.

    For TX the load impedance will change a lot since C181 has a large impact on the impedance. The output power and harmonics will be different.

    The TRX pin has to be connected when the RX and TX paths are combined. If RX and TX are split in two independent paths connection to the TRX pin may be omitted.