Other Parts Discussed in Thread: CC1101, TPS62730
Dear TI E2E Community,
I don't find on Datasheet what AVDD ad DVDD pin supply internally to the chip. My target is to reduce as much as possible the battery consumption.
My idea is to separate AVDD with 2,1V and DVDD with 3,3V same as MCU (fixed);
My question are:
1) After chipset inizialization (write), may I switch off 2,1V AVDD to reduce the battery power consumption (during sleep mode of mcu) and keep the register contenents?
2) When the mcu wakeup, and processing need to transmit data may I switch on 2,1V AVDD and strobe in TX mode the CC1101?
Is there any wrong procedure in the 2 steps to save the battery consumption?
3) There are some advantages separating AVDD and DVDD for the point of view of power consumption if i can switch off 2,1V?
Unfortunatly it is impossible separate on CC1101EVM AVDD and DVVD to test if there any reduction in power consumption.
Is there any document not listed under CC1101 Application Note that can explain better AVDD and DVDD difference?
Thank you