This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCStudio SmartRF06/CC2538EM connectivity problems

Other Parts Discussed in Thread: CC2538

Hi,

I can create and build the default project for a CC2538 using CCS. When I attempt to debug the project I get the following error:

"Error connecting to the target:
(Error -233 @ 0x0)
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
(Emulation package 5.1.73.0)"

The SmartRF Flash Programmer 2 recognizes the device OK and I can debug using the IAR IDE without any problems.

Any ideas?

Thanks, Steve