Hello,
I am trying to program the TRF7970a EVM using CCSv5. I want this EVM to communicate with the tablet Nexus 7. There are some problems with debugging.
1. When this EVM is connected to the PC via MSP40-JTAG-TINY, it does not detect any tag. (Whereas, if connected to PC via USB, it detects the tag successfully.) Plus, when connected via JTAG, the program runs very slowly (checked by setting an LED on and off). What could be the reason?
2. I would like to set the EVM as a target and poll for any external RF field(e.g. from tablet). I am very confused about how to do that and not getting started with this. Which would be the appropriate functions to be used from the firmware?
I hope someone can shed a light on this. Thank you.
Regards.