We have a design using a TRF7960a connected to a MSP430F5438a.
We have a problem with the oscillator. We can se on the TRF7960_EVM_revA as soon as the EN pin is raised the oscillator starts to oscillate at 13.560MHz as anyone would expect.
On our design, when we raise the same EN pin, we simply see ~1.8Vdc on each side of our crystal, but it doesn't oscillate.
We use a Abracom 13.560MHz crystal, with a load capacitance of 18pF and an ESR of 80R.
The reference board as a 13.56MHz crystal with a load capacitance of 12pF and an ESR of 30R on it. (http://www.abracon.com/Resonators/ABM8G.pdf)
Can this be enough difference to prohibit our oscillator from operating normaly?
I am attaching our TRF7960a schematic page, just in case you guys notice something out of the ordinary.