Hello:
I have the CC1111EMK868-915 Evaluation Module Kit and am using TI's SmartRF Protocol Packet Sniffer software to monitor some devices my employer is bringing to market. To provide a documentation trail for the eventual approval of the end device, I need to use the file captured by the sniffer during the end product tests. I can provide the auditor documentation on every data field in the PSD file since the documentation on the PSD file format is clear about what fields are embedded where, the length of the fields, the byte orientation of multi byte values, etc. However, while the documentation is clear that the timestamp embedded with the packet will need to be divided by a clock value that is specific to hardware, I cannot find this value documented anywhere.
Can someone tell me what the clock value of the CC1111EMK868-915 Evaluation Module Kit is and provide a reference I can include in the audit package?
Thanks
Mike