Other Parts Discussed in Thread: CC1101, CC1125, CC1120
Comparing the sensitivity figures of the CC1125 and the CC1101 I see they are specified differently: the CC1125 figures are for a 1% BER whereas those for the CC1101 are at 1%, 20 byte packet error rate. I calculate the latter to 1% of 20 * 8 = 160 bits which is a BER of 6.25 x 10^-5.
Looking at some BER/SNR plots for FSK it appears to mean the CC1125 sensitivity figures need to be reduced by about 5dB to be comparable to those of the CC1101.
Is this correct or am I missing something obvious? What value should I be using to adjust for the differing BERs? I'm most interested in 38.4kb/s GFSK at 434MHz where the specified values are -110dB (CC1125), -104dB (CC1101) which would mean very similar sensitivities.
Thanks,
Tony H