Hello,
We are working on RTLS based vehicle tracking.
System Description : We have TI MSP-EXPCC430RF4 evolution kit. In this system, there are 3 devices which are End device(CC430F5137-satellite board) ,
Sub-controller(CC430F6137-base board) and Master device(CC430F6137-base board).
End devices will continuously send data to sub-controllers.Sub-controllers will calculate RSSI value of End device.
Sub-controllers will send this RSSI value to master device.Using this RSSI value,we will measure distance between sub-controllers and End device.
Master device is connected to PC where we can see the position of End device.
We are using simpliciTi stack for this system.
As per "SimpliciTI Change Log" of simpliciTi, we may not get RSSI value consistent.
I have attached "SimpliciTi Change Log" file in this post.
6507.simpliciTi_change_log.pdf
Anybody has working on that known issue and is it fixed or not?
Thanks & Regards,
Chetan Panchal