Hi,
I have a HomeAgain (http://microchip.homeagain.com/) transponder which is claimed to operate at 134.2 kHz according to ISO specs (I imagine they mean ISO 11784 & 11785). I also have the TMS3705 hooked up with an antenna outputting 134.45 kHz, >50V at the capacitor/coil junction.
When reading the SCIO pin the IC sends the 0xAF byte indicating that the antenna is working. Finally, following the 0xAF byte, the IC sends a 19 byte data series (after extracting each byte from the start, and end 1 and 0, respectively, flipping each byte, and inverting them).
The problem is that it sends this data (I didn't check whether it was consistent) whether my transponder is present or not. So I have to assume it just garbage. Still I'm curious why 19 bytes. Anyway, I read somewhere that this transponder uses FDX-B, so the first question is whether TMS3705 supports FDX?
Assuming it is FDX, I should see the transponder response while the IC is charging it. But, again, whether the transponder is present, there are 50+mv variations in the amplitude of the coil voltage, so maybe that's where the IC gets the 19 bytes. I tested also with a large ID card which is a 125 kHz transponder, but I could see no changes between the transponder being present or absent. For both transponders I also watched for changes above noise after the IC stops the antenna, in case it's HDX, but nothing.
So my question is about the FDX support. But also, is noise this large expected in the coil?
P.S. When I looked at the fft of the coil wave, there as a giant spike at 134 kHz, but also two large side lobes at ~120 kHz and ~160kHz range. There were also smaller, but regular spikes at every tens of kHz or so.
Thanks!