Hey guys,
I've got a huge problem with such an ADR2. I need to use that board with LabView, its a programming language from NI.
My connectivity is made up with RS232. So when I use the RFID-Demo Software especially for the ADR2 it mostly works fine. I don't know what kind of COM-Settings are made but it works.
When I try to use the ADR2 with my LabView programm sometimes its working sometimes not. Mostly right after using the RFID-Demo it works also within my programm. But thats not a solution and its not even working always.
When I try to get the device ID from a assembly, I send him: 010884021410F002000A72
Mostly I recieve: 010B0000000000... but also some fragments from the write part...
Thats the code I expect to recieve: 010B007E1AF81C07B0F30204A168
Does anybody know the complete Serial Configuration Settings of this ADR2 ?