I just ordered a CC2540EMK-USB kit from Digikey and installed the SmartRF Protocol Packet Sniffer on a Windows XP 32-bit machine (SP2) with USB 2.0 ports.
Unfortunately, the sniffer software does not show the CC2540 when I select "Bluetooth Low Energy" and start that sniffer program.
Under Windows Device Manager, I see the USB trident and then "Cebal controlled devices". A singular child node of this has another USB trident and then "CC2540 USB dongle". I have tried updating the driver with the one found in the C:\Program Files\Texas Instruments\SmartRF Tools\Drivers\cebal\win_32bit_x86\cebal2.inf
Also, multiple reboots and plug/unplug permutations have not solved the problem.
Could my CC2540EMK-USB have come from the factory without the proper firmware loaded on it? Argh, frustration!
--- Zach