Hi,
I am trying to flash my CC1111 on my Windows 7 (64-bit) via the CC Debugger, but I can't establish a proper target connection. The led of the CC Debugger is always red.
First off, here's my setup:
- pin #1 of the CC Debugger is connected to pin #1 of the CC1111.
- Both USB devices (Debugger & CC1111) are powered by the USB bus
- Both USB devices come up with the proper USB vendor / dev id (vendor: 0x0451 / dev: 0x16ad and dev: 0x16a2), and are visible in the Windows device manager
Starting SmartRF Studio 7 (1.13.0) shows only the CC Debugger as connected device with the folloeing line:
CC Debugger (USB device ID=0000, Firmware revision=0041), -- no chip
The only weird thing is the device ID 0000 of the CC Debugger?!?
Does anybody have a good idea how to debug / proceed further? I just got these 2 TI devices last week and desperately need them for work...
Kind Regards,
Artur
PS: I can successfully flash the CC Debugger with the latest greatest firmware.