Hello,
I'm trying to configure the CC1101 to receive an existing protocol. This protocol is Manchester encoded and uses the sync word 0xAF, followed by the packet length. With this protocol not using at least a 16 bit sync word, can I use the build-in packet handler, and if so, do I need to manually encode the sync word to configure it in the SYNC1 and SYNC0 registers?
Thanks in advance!