Other Parts Discussed in Thread: CC1120
We are designing a new product that may be appropriate for the CC1120 or another chip in the family. I want to be able to do the following:
1.) Set the product in Receive mode but turn on the PA amplifier to create a un modulated RF signal. Is there an option bit to allow this feature
2.) The product doesn't support the encoding desired. Is it p[ossilbe to load the FIFO with encoded data patterns which will directly modulate the RF carrier (ASK modulation is appropriate with the existing options)
3.) Likewise can the raw un decoded data be loaded into the FIFO for MPU decoding?
We would like to dicuss our needs further offline