Hallo
In the user guide is written "It is also possible to disconnect the MSP430F2370 from the TRF7970A and use these headers to wire in another MCU (for example, other members of the MSP430™, Stellaris™ Cortex™-M3, or Sitara™
ARM8™ and ARM9™ families)."
I have just one small question: How?
I want to use another MCU and they should communicate via SPI.
I already did this: "To change to SPI with Slave Select operation, move all the 0-Ω resistors connecting HDR_4 and HDR_5 together so that HDR_5 and HDR_6 are connected and move the 0-Ω resistor on HDR_7 so that I/O_SEL and SPI are connected instead."
Are the TRF7970A and the MCU are now disconnected?
Thank and best regards
Flo