I've inherited a project that is using the CC1101. The issue is that the software is programing the power output at 433MHz with 0x77 which does not exist in the PATABLE. (This is a software bug left over from when a CC1150 was being used.) The question I have is what power output in dBm should I expect at 433MHz when programming the chip with 0x77?