Hello,
I have not been able to achieve the sensitivity and adjacent channel rejection performance reported in application note AN122. To measure the sensitivity I am using the CC1125 Cat 1 development boards for a transmitter and receiver. The dev boards are placed in metal boxes to minimise radiated signals. An RF cable runs between the two boxes and I insert RF attenuators in the conducted path to reduce the signal until the sensitivty limit is reached. Using ETSI CAT1 869MHz 4.8kbps settings from RF studio (Ver 1.14.1) I can only achieve -109dBm sensitivity rather than the -115dBm expected.
I am also not achieving the adjacent channel rejection reported in AN122. My results are about 10dB worse than expected.
Is there anything obvious that I may be missing?