Hello people of the E2E Community ;),
I’ve got a question about that Demo Reader Board.
It is getting supplied with 12V over a relay and sometimes it is even not reacting to the RFID Demo Software of TI. The software is starting to set up a connection with three specific commands:
1. (is optional) Get SerialNumber
TX: 01010504
RX: 010505020804010F
2. (needed) I guess its a activation code
TX: 010D170154009600A0009600FA009683
RX: 010D190154009600A0009600FA00968D
3. (needed) same as 2
TX: 010B1B01AE009604B000AA100126
RX: 010B1D01AE009604B000AA100120
But sometimes it is not even responding to one of those commands. Only if I unplug the main power supply of our complete system and plug it in again after a little delay of three seconds. Then it is able to react on those three commands and everything works fine again.
Is this a known issue and do you have any advice to solve this problem?
hope anybody can help me to solve my issue,
Dave