Hi everyone! First of all, let me apologize for being very inexperienced in RF design/applications, I am more of a DSP guy. This is also my first forum post here.
My problem is this: I am looking into the possibility of using time-difference-of-arrival (TDOA) to trilaterate a signal source at an unknown location by determining the TDOA between 3 different base stations at known positions.
The base stations and the transmitters will both be using the CC1125 transceiver at 169 MHz. The base stations will use a GPS-based time references. The method i want to investigate is as follows:
- GPS 1 pulse-per-second at base station triggers counter.
- Counter starts counting pulses from a 100MHz OCXO
- Receiver (CC1125) picks up signal from transmitter
- Stop counter/load count value into register.
The count value will represent a time reference for when the transceiver picked up a signal from the transmitter, and comparison between base stations lets me calculate its position.
The crucial point is: how can I implement a "trigger" from the CC1125? Something that can be used to uniquely timestamp the signal.
I am very new to this, but could it be possible to set an output pin high at the end of the preamble, or something to that effect?
I am an electronics student, and this is my final year project.
Thanks for any answers, and kind regards
Snorre