This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200

Other Parts Discussed in Thread: CC1200, CC1120

design guide of CC1200 for 138MHz, and 460MHz, I need TX & RX attenna separately

  • There are 169 MHz and 420-470 MHz reference designs on web.

    420-470 MHz: http://www.ti.com/tool/cc1200em-420-470-rd

    169 MHz: http://www.ti.com/tool/cc1120em-169-rd. This is for CC1120, but you can use this and simply change to CC1200 and use 40 MHz crystal. This design can be used as a starting point and might need to be tweaked for optimum performance at 138 MHz.

    For dual band operation you need to add switches to the design and there will be a few passives as you need separate balun and PA load for the two frequency bands. A sketch is attached - use 169 MHz design instead of 868 MHz.

    2656.Dual Band 2 switches.pdf

  • Hello,

    I’m currently working on fast switch from Tx to Rx state without intermediate IDLE state and I have the following questions:

    1)      Do I need to clear PA_POWER_RAMP=0 when I use Tx/Rx turnaround?

    2)      When ramp-down operation starts and stops when I use Tx/Rx turnaround (command strobe SRX)?

    3)      Does Tx/Rx turnaround guarantee a sterling Tx->Rx switch: I can see that Rx_Fifo must be flushed?

    4)      What side effect could I face when I send the command strobe SFRX in Rx state?

    Thanks a lot,

    Alex