Hi all,
from this application note I have extracted the following figures, not related to my current work :)
However, as you can see, in all of them the trace from / to SMA antenna plug is drawn as wider than the rest. This is not my work area but I want to design a low-power board as well as possible. Hope you can help me with some questions! :)
In the board I'm designing, I'm working at 868MHz. All the components are connected by 0.3mm traces. I know the impedance of the previously mentioned SMA trace is related to its width, which will be probably higher than 0.3mm. In my board, just after the SMA trace there is a 0603 inductor which is part of an impedance matching network. Thus, when drawing my board in EAGLE, I find that the width of the SMA trace should be kind of assymetric, since the SMA side is much wider than the pad of the 0603 component I want it to be attached to.
So, my questions are:
- Which is the trace width you use to employ for SMA traces? Since the SMA center pin is considerable in size, I guess for maximum energy transfer the trace coming out of it has to be bigger, as in the pictures I attached.
- Which is the correct way to design this? Keeping the SMA trace as short as possible to make it affect the impedance matching as few as possible, or allow the SMA trace to have a length of 1cm for example and re-do my impedance calculations taking this into account? The value of the 0603 inductor is known but right now I do not have the paper here :(
Ok, eagering to know your opinions! I have searched the forum for something similar to this but I was not able (yet) to extract related information, if any :)