Other Parts Discussed in Thread: CC1101
Hi,
I am using the IC CC1101 applicatication circuit shown in its specification to make a 868MHz Transiver unit. Please see the photo above: the yellow line is from my module at TX mode and the green is from another vendor's module (CC1101 also) at TX mode.
My questions are as below:
1)Why do the two modules have RF power at the marks of 2 and 3 at TX mode? Is it normal?
2)How to decrease them?
3)When the two modules are changed to RX mode, the vendor's module has a higher sensitivity than mine at the same test conditions. Please be noted from the photo above that the vendor's module has lower RF power at the marks of 2 and 3 than mine. Does the receiving sensitivity at RX mode has the direct relation with the RF power at the marks of 2 and 3 at TX mode in the same module with CC1101?
Please kindly help.
Many thanks
Jacky