I just received two TRF7960ATB boards via DigiKey and both has the wrong Regulator on them.
They are designed to have the tps61222DCKT on them which is a fixed 5.0V boost.
But instead they had the tps61222DCKR which is adjustable.
I tried to work with Ti customer support on this and after a week and taking picture of the issue, they claim the board is correct.
Has anyone else had issues with the build of the board or EVM boards?
Did TI do anything about it?
Is there a better options for RFID then TI?