This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200 - best layer stack-up in case of 6 or 8 layers

Other Parts Discussed in Thread: CC1200

Hi,

I'm designing an RF transceiver based on the CC1200 chip.

The board will have a board-to-board connector and will be a daughter board.

The product will have the following parts:

- CC1200

- IPC matching component

- SAW filter

- SMA and-launch connector

- 8-pin board-to-board connector with the SPI interface, power, ground, reset and 1 GPIO pin

The board will have the following dimensions:  20 mm x 10 mm (390 x 780 mils)

The board will have a metal shield.

QUESTION 1

-----------------

What would be the best layer stack-up in case of 6 layers?

QUESTION 2

-----------------

What would be the best layer stack-up in case of 8 layers?

Thanks in advance,

Enrico Migliore