This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1120 Deviation vs Xtal accuracy

Hello.

I´m developing a system with this transceiver. I have configured the registers with Smart RF Studio, that I supposed that are values for a 10ppm xtal ("32MHz). My settings are for 868MHz, 50kbps, 2-GFSK, one of the predefined options of Smart RF Studio.

My question is, if I get a deviation of 25KHz for 10ppm xtal, can I use a 2ppm xtal to reduce the deviation and improve  the sensitivity? Or it exists a limitation to reduce the deviation?

If its ok, can I  use a 5KHz deviation for 2ppm?

Thanks for the answers

Jose