This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem transferring single integer data from End Device to Access Point, EZ430rf2500



I have purchased one EZ430RF2500. My application includes transfer of sampled (@20KHz, 10 bit) analog data between the ED and the AP. I have started with modifying the Sensor demo example to move towards my objective.

I have modified the main_AP.c and main_ED.c to remove the ADC function altogether from both the files. Instead I am sending only an integer value (99).  Also I have decreased the value of TACCR0 to 30. AS the debugger operates at a maximum rate of 9600 bps, we are using a UART to USB bridge converter to increase the data transfer rate between the AP and the PC. Further I have changed the baud rate setting from 9600 to 115200.

I am using a software 'terminal' to log the data received at the COM port of the PC.

But still I am receiving data in the in the previous format as follow: $0001,-34.5F,4.4,032,N#<0>

I cannot find the integer (99) in the received data. I am pasting the modified main_ED.c below:

#include "bsp.h"
#include "mrfi.h"
#include "nwk_types.h"
#include "nwk_api.h"
#include "bsp_leds.h"
#include "bsp_buttons.h"
#include "vlo_rand.h"

/*------------------------------------------------------------------------------
 * Defines
 *----------------------------------------------------------------------------*/
/* How many times to try a TX and miss an acknowledge before doing a scan */
#define MISSES_IN_A_ROW  2

/*------------------------------------------------------------------------------
 * Prototypes
 *----------------------------------------------------------------------------*/
static void linkTo(void);
void createRandomAddress(void);
__interrupt void ADC10_ISR(void);
__interrupt void Timer_A (void);

/*------------------------------------------------------------------------------
* Globals
------------------------------------------------------------------------------*/
static linkID_t sLinkID1 = 0;
/* Temperature offset set at production */
volatile int * tempOffset = (int *)0x10F4;
/* Initialize radio address location */
char * Flash_Addr = (char *)0x10F0;
/* Work loop semaphores */
static volatile uint8_t sSelfMeasureSem = 0;

/*------------------------------------------------------------------------------
 * Main
 *----------------------------------------------------------------------------*/
void main (void)
{
  addr_t lAddr;

  /* Initialize board-specific hardware */
  BSP_Init();

  /* Check flash for previously stored address */
  if(Flash_Addr[0] == 0xFF && Flash_Addr[1] == 0xFF &&
     Flash_Addr[2] == 0xFF && Flash_Addr[3] == 0xFF )
  {
    createRandomAddress(); // Create and store a new random address
  }

  /* Read out address from flash */
  lAddr.addr[0] = Flash_Addr[0];
  //lAddr.addr[1] = Flash_Addr[1];
  //lAddr.addr[2] = Flash_Addr[2];
  //lAddr.addr[3] = Flash_Addr[3];

  /* Tell network stack the device address */
  SMPL_Ioctl(IOCTL_OBJ_ADDR, IOCTL_ACT_SET, &lAddr);

  /* Initialize TimerA and oscillator */
  //DCOCLT |=DCO2;
  //BCSCTL2|=
  BCSCTL3 |= LFXT1S_2;                      // LFXT1 = VLO
  TACCTL0 = CCIE;                           // TACCR0 interrupt enabled
  TACCR0 = 30;                           // ~ 0.025 sec
  TACTL = TASSEL_1 + MC_1;                  // ACLK, upmode

  /* Keep trying to join (a side effect of successful initialization) until
   * successful. Toggle LEDS to indicate that joining has not occurred.
   */
  while (SMPL_SUCCESS != SMPL_Init(0))
  {
    BSP_TOGGLE_LED1();
    BSP_TOGGLE_LED2();
    /* Go to sleep (LPM3 with interrupts enabled)
     * Timer A0 interrupt will wake CPU up every second to retry initializing
     */
    __bis_SR_register(LPM3_bits+GIE);  // LPM3 with interrupts enabled
  }

  /* LEDs on solid to indicate successful join. */
  BSP_TURN_ON_LED1();
  BSP_TURN_ON_LED2();

  /* Unconditional link to AP which is listening due to successful join. */
  linkTo();

  while(1);
}

static void linkTo()
{
  uint8_t msg[1];
#ifdef APP_AUTO_ACK
  uint8_t misses, done;
#endif

  /* Keep trying to link... */
  while (SMPL_SUCCESS != SMPL_Link(&sLinkID1))
  {
    BSP_TOGGLE_LED1();
    BSP_TOGGLE_LED2();
    /* Go to sleep (LPM3 with interrupts enabled)
     * Timer A0 interrupt will wake CPU up every second to retry linking
     */
    __bis_SR_register(LPM3_bits+GIE);
  }

  /* Turn off LEDs. */
  BSP_TURN_OFF_LED1();
  BSP_TURN_OFF_LED2();

  /* Put the radio to sleep */
  SMPL_Ioctl(IOCTL_OBJ_RADIO, IOCTL_ACT_RADIO_SLEEP, 0);

  while (1)
  {
    /* Go to sleep, waiting for interrupt every second to acquire data */
    __bis_SR_register(LPM3_bits);

    /* Time to measure */
    if (sSelfMeasureSem) {
      //volatile long temp;
      //int volt;
      //int results[1];
#ifdef APP_AUTO_ACK
      uint8_t      noAck;
      smplStatus_t rc;
#endif

      
      /* Get voltage */
     // ADC10CTL1 = INCH_0 + ADC10DIV_4;                     // AVcc/2 ADC10CLK/5
      //ADC10CTL0 = SREF_1 + ADC10SHT_2 + REFON + ADC10ON + ADC10IE + REF2_5V;
     // __delay_cycles(240);
     // ADC10CTL0 |= ENC + ADC10SC;             // Sampling and conversion start
      //__bis_SR_register(CPUOFF + GIE);        // LPM0 with interrupts enabled
      //results[0] = ADC10MEM;                  // Retrieve result

      /* Stop and turn off ADC */
     //ADC10CTL0 &= ~ENC;
      //ADC10CTL0 &= ~(REFON + ADC10ON);

      

      /* message format,  UB = upper Byte, LB = lower Byte
      -------------------------------
      |degC LB | degC UB |  volt LB |
      -------------------------------
         0         1          2
      */
      //temp = results[0];
      //volt = (temp*25)/512;
      msg[0] = 99;//volt;
      /*msg[1] = 1;
      msg[2] = 2;
      msg[3] = 3;
      msg[4] = 4;
      msg[5] = 5;
      msg[6] = 6;
      msg[7] = 7;
      msg[8] = 8;
      msg[9] = 9;*/
      

      /* Get radio ready...awakens in idle state */
      SMPL_Ioctl( IOCTL_OBJ_RADIO, IOCTL_ACT_RADIO_AWAKE, 0);

#ifdef APP_AUTO_ACK
      /* Request that the AP sends an ACK back to confirm data transmission
       * Note: Enabling this section more than DOUBLES the current consumption
       *       due to the amount of time  RX waiting for the AP to respond
       */
      done = 0;
      while (!done)
      {
        noAck = 0;

        /* Try sending message MISSES_IN_A_ROW times looking for ack */
        for (misses=0; misses < MISSES_IN_A_ROW; ++misses)
        {
          if (SMPL_SUCCESS == (rc=SMPL_SendOpt(sLinkID1, msg, sizeof(msg), SMPL_TXOPTION_ACKREQ)))
          {
            /* Message acked. We're done. Toggle LED 1 to indicate ack received. */
            BSP_TURN_ON_LED1();
            __delay_cycles(2000);
            BSP_TURN_OFF_LED1();
            break;
          }
          if (SMPL_NO_ACK == rc)
          {
            /* Count ack failures. Could also fail becuase of CCA and
             * we don't want to scan in this case.
             */
            noAck++;
          }
        }
        if (MISSES_IN_A_ROW == noAck)
        {
          /* Message not acked */
          BSP_TURN_ON_LED2();
          __delay_cycles(2000);
          BSP_TURN_OFF_LED2();
#ifdef FREQUENCY_AGILITY
          /* Assume we're on the wrong channel so look for channel by
           * using the Ping to initiate a scan when it gets no reply. With
           * a successful ping try sending the message again. Otherwise,
           * for any error we get we will wait until the next button
           * press to try again.
           */
          if (SMPL_SUCCESS != SMPL_Ping(sLinkID1))
          {
            done = 1;
          }
#else
          done = 1;
#endif  /* FREQUENCY_AGILITY */
        }
        else
        {
          /* Got the ack or we don't care. We're done. */
          done = 1;
        }
      }
#else

      /* No AP acknowledgement, just send a single message to the AP */
      SMPL_SendOpt(sLinkID1, msg, sizeof(msg), SMPL_TXOPTION_NONE);

#endif /* APP_AUTO_ACK */

      /* Put radio back to sleep */
      SMPL_Ioctl( IOCTL_OBJ_RADIO, IOCTL_ACT_RADIO_SLEEP, 0);

      /* Done with measurement, disable measure flag */
      sSelfMeasureSem = 0;
    }
  }
}

void createRandomAddress()
{
  unsigned int rand;//, rand2;
  do
  {
    rand = TI_getRandomIntegerFromVLO();    // first byte can not be 0x00 of 0xFF
  }
  while( (rand & 0xFF00)==0xFF00 || (rand & 0xFF00)==0x0000 );
  //rand2 = TI_getRandomIntegerFromVLO();

  BCSCTL1 = CALBC1_1MHZ;                    // Set DCO to 1MHz
  DCOCTL = CALDCO_1MHZ;
  FCTL2 = FWKEY + FSSEL0 + FN1;             // MCLK/3 for Flash Timing Generator
  FCTL3 = FWKEY + LOCKA;                    // Clear LOCK & LOCKA bits
  FCTL1 = FWKEY + WRT;                      // Set WRT bit for write operation

  Flash_Addr[0]=(rand>>8) & 0xFF;
  //Flash_Addr[1]=rand & 0xFF;
  //Flash_Addr[2]=(rand2>>8) & 0xFF;
  //Flash_Addr[3]=rand2 & 0xFF;

  FCTL1 = FWKEY;                            // Clear WRT bit
  FCTL3 = FWKEY + LOCKA + LOCK;             // Set LOCK & LOCKA bit
}

/*------------------------------------------------------------------------------
 * ADC10 interrupt service routine
 *----------------------------------------------------------------------------*/
//#pragma vector=ADC10_VECTOR
//__interrupt void ADC10_ISR(void)
//{
 // __bic_SR_register_on_exit(CPUOFF);        // Clear CPUOFF bit from 0(SR)
//}

/*------------------------------------------------------------------------------
 * Timer A0 interrupt service routine
 *----------------------------------------------------------------------------*/
#pragma vector=TIMERA0_VECTOR
__interrupt void Timer_A (void)
{
  sSelfMeasureSem = 1;
  __bic_SR_register_on_exit(LPM3_bits);        // Clear LPM3 bit from 0(SR)
}

Why am I not getting the integer in the received data? Why the old data format is still followed? The modified data is supposed to send only a single integer value. But why is it not?

Soliciting help. Thanks in advance.

  • Have you modified the code on the AP side? It will parse the incoming packet and convert the integers you send to what it believes are temperature and voltage readings on the ED side. Change the AP code to write exactly what you receive to the com port.