This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with upgrading from cc2500 to cc1101

Other Parts Discussed in Thread: TEST2, CC1101, CC2500

Hi,

 So far I used cc2500em transceiver msp430f5529 evaluation board with the following settings : RF frequency 2400 MHz, MSK modulation, 250 kbps data rate, 540kHz rx filterbandwidth ( I attached the register setup code) when I used that setting everything worked fine, but when I started to use cc1101em transceiver with the following settings: RF frequency 868 MHz, MSK modulation, 250 kbps data rate, 540kHz rx filterbandwidth ( I attached the register setup code for it to) I succeed to receive several message from the sender and after several message the sender got stuck on the line code :

 "while (!(TI_CC_GDO0_PxIN&TI_CC_GDO0_PIN));" of the the attached RFSendPacket function and stop sending messages. I will be glad if someone may have any ideas what may cause it and what should I do for solving it.

Thanks

Roy

void RFSendPacket(char *txBuffer, char size)
{
TI_CC_SPIWriteBurstReg(TI_CCxxx0_TXFIFO, txBuffer, size); // Write TX data
TI_CC_SPIStrobe(TI_CCxxx0_STX); // Change state to TX, initiating
// data transfer

while (!(TI_CC_GDO0_PxIN&TI_CC_GDO0_PIN));
// Wait GDO0 to go hi -> sync TX'ed
while (TI_CC_GDO0_PxIN&TI_CC_GDO0_PIN);
// Wait GDO0 to clear -> end of pkt
TI_CC_GDO0_PxIFG &= ~TI_CC_GDO0_PIN; // After pkt TX, this flag is set.
// Has to be cleared before existing
}

my CC2500 register setting:

void writeRFSettings(void)
{
// Write register settings
TI_CC_SPIWriteReg(TI_CCxxx0_IOCFG2, 0x0B); // GDO2 output pin config.
TI_CC_SPIWriteReg(TI_CCxxx0_IOCFG0, 0x06); // GDO0 output pin config.
TI_CC_SPIWriteReg(TI_CCxxx0_PKTLEN, 0xFF); // Packet length.
TI_CC_SPIWriteReg(TI_CCxxx0_PKTCTRL1, 0x05); // Packet automation control.
TI_CC_SPIWriteReg(TI_CCxxx0_PKTCTRL0, 0x05); // Packet automation control.
TI_CC_SPIWriteReg(TI_CCxxx0_ADDR, 0x01); // Device address.
TI_CC_SPIWriteReg(TI_CCxxx0_CHANNR, 0x00); // Channel number.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCTRL1, 0x07); // Freq synthesizer control.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCTRL0, 0x00); // Freq synthesizer control.
TI_CC_SPIWriteReg(TI_CCxxx0_FREQ2, 0x5D); // Freq control word, high byte
TI_CC_SPIWriteReg(TI_CCxxx0_FREQ1, 0x93); // Freq control word, mid byte.
TI_CC_SPIWriteReg(TI_CCxxx0_FREQ0, 0xB1); // Freq control word, low byte.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG4, 0x2D); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG3, 0x3B); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG2, 0x73); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG1, 0x22); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG0, 0xF8); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_DEVIATN, 0x00); // Modem dev (when FSK mod en)
TI_CC_SPIWriteReg(TI_CCxxx0_MCSM1 , 0x3F); //MainRadio Cntrl State Machine
TI_CC_SPIWriteReg(TI_CCxxx0_MCSM0 , 0x18); //MainRadio Cntrl State Machine
TI_CC_SPIWriteReg(TI_CCxxx0_FOCCFG, 0x1D); // Freq Offset Compens. Config
TI_CC_SPIWriteReg(TI_CCxxx0_BSCFG, 0x1C); // Bit synchronization config.
TI_CC_SPIWriteReg(TI_CCxxx0_AGCCTRL2, 0xC7); // AGC control.
TI_CC_SPIWriteReg(TI_CCxxx0_AGCCTRL1, 0x00); // AGC control.
TI_CC_SPIWriteReg(TI_CCxxx0_AGCCTRL0, 0xB2); // AGC control.
TI_CC_SPIWriteReg(TI_CCxxx0_FREND1, 0xB6); // Front end RX configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_FREND0, 0x10); // Front end RX configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL3, 0xEA); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL2, 0x0A); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL1, 0x00); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL0, 0x11); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSTEST, 0x59); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_TEST2, 0x88); // Various test settings.
TI_CC_SPIWriteReg(TI_CCxxx0_TEST1, 0x31); // Various test settings.
TI_CC_SPIWriteReg(TI_CCxxx0_TEST0, 0x0B); // Various test settings.
}

// PATABLE (0 dBm output power)
extern char paTable[] = {0xFB};
extern char paTableLen = 1;

my CC1101 register setting:

void writeRFSettings(void)
{
// Write register settings

TI_CC_SPIWriteReg(TI_CCxxx0_IOCFG2, 0x0B); // GDO2 output pin config.
TI_CC_SPIWriteReg(TI_CCxxx0_IOCFG0, 0x06); // GDO0 output pin config.
TI_CC_SPIWriteReg(TI_CCxxx0_PKTLEN, 0xFF); // Packet length.
TI_CC_SPIWriteReg(TI_CCxxx0_PKTCTRL1, 0x05); // Packet automation control.
TI_CC_SPIWriteReg(TI_CCxxx0_PKTCTRL0, 0x05); // Packet automation control.
TI_CC_SPIWriteReg(TI_CCxxx0_ADDR, 0x01); // Device address.
TI_CC_SPIWriteReg(TI_CCxxx0_CHANNR, 0x00); // Channel number.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCTRL1, 0x0C); // Freq synthesizer control.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCTRL0, 0x00); // Freq synthesizer control.
TI_CC_SPIWriteReg(TI_CCxxx0_FREQ2, 0x21); // Freq control word, high byte
TI_CC_SPIWriteReg(TI_CCxxx0_FREQ1, 0x62); // Freq control word, mid byte.
TI_CC_SPIWriteReg(TI_CCxxx0_FREQ0, 0x76); // Freq control word, low byte.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG4, 0x2D); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG3, 0x3B); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG2, 0x73); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG1, 0x22); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG0, 0xF8); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_DEVIATN, 0x60); // Modem dev (when FSK mod en)
TI_CC_SPIWriteReg(TI_CCxxx0_MCSM1 , 0x3F); //MainRadio Cntrl State Machine
TI_CC_SPIWriteReg(TI_CCxxx0_MCSM0 , 0x18); //MainRadio Cntrl State Machine
TI_CC_SPIWriteReg(TI_CCxxx0_FOCCFG, 0x1D); // Freq Offset Compens. Config
TI_CC_SPIWriteReg(TI_CCxxx0_BSCFG, 0x1C); // Bit synchronization config.
TI_CC_SPIWriteReg(TI_CCxxx0_AGCCTRL2, 0xC7); // AGC control.
TI_CC_SPIWriteReg(TI_CCxxx0_AGCCTRL1, 0x00); // AGC control.
TI_CC_SPIWriteReg(TI_CCxxx0_AGCCTRL0, 0xB0); // AGC control.
TI_CC_SPIWriteReg(TI_CCxxx0_FREND1, 0xB6); // Front end RX configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_FREND0, 0x10); // Front end RX configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL3, 0xEA); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL2, 0x2A); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL1, 0x00); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL0, 0x1F); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSTEST, 0x59); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_TEST2, 0x88); // Various test settings.
TI_CC_SPIWriteReg(TI_CCxxx0_TEST1, 0x31); // Various test settings.
TI_CC_SPIWriteReg(TI_CCxxx0_TEST0, 0x09); // Various test settings.

}

// PATABLE (0 dBm output power)
extern char paTable[] = {0x50};
extern char paTableLen = 1;