Dear Sir,
The reference design of the CC2592 is based on the CC2538. Our design is based on the CC2541 including the CC2592. The CC2541 likes to see another load impedance at its differential RF ports as the CC2538.
The reference deisgn based on the CC2538 advises to take over the component distance and trace prperties. Is this still the case when using the CC2541? What is your experiamce when using the CC2541 instead of the CC2528.
M. Struik