I did post this question at the end of another thread but was not sure if it would be read, so I created another posting.
I would like to increase the operating range of the microreader. I have tried larger antennas - a 200mm x 900mm antennas gives me around 600mm read range with a large 70mm diameter tag antenna, but can I increase the range further using similar techniques to those outlined in SCBA031, i.e. adding an external driver stage. I guess there are two questions here - (a) will that approach work to increase down link power and (b) will the micro reader have sufficient sensitivity?