FS_CHP_RESERVED5_0 0x28 R/W For test purposes only, use values from SmartRF Studio
I have two evaluation kits, and each has a different value in SmartRF Studio for the above register. One has a value of 0x07 and the other is 0x08. The are several other "test purposes only" registers that also differ between boards (AGC_GAINx, FS_VCO4, etc...). What value should I use in my register initialization for these registers, or should all these values be left at their default values rather than the SmartRF Studio value?
Thanks.