This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Stack size

Other Parts Discussed in Thread: CC2543

Hi,

I am working on CC2543..

These lines from the map file when I compile it:

16 104 bytes of CODE memory

18 bytes of DATA memory (+ 54 absolute )
745 bytes of XDATA memory (+ 128 absolute )
64 bytes of IDATA memory
8 bits of BIT memory

after that I extend one global array by 40 bytes, I get: error:

Error[e16]: Segment XDATA_Z (size: 0x225 align: 0) is too long for segment definition. At least 0x26 more bytes needed. The problem occurred while processing the segment placement command...

I tried to go to General Options --> Stack/Heap --> Stack Sizes and to increase the XDATA from 0x100 to 0x130 or 0x200 or 0x300 but it does not help.

can you help me please what can I do?

Thanks.