Hi all,
In order to evaluate the 14443 Type B card emulation using TRF7970A, I have ported the example code '6507.Card Emulation TRF7970EVM Parallel Mode Jan 7' to TRF7970A EVM Rev.A and tried to read using several readers. The EVM is unable to enter the ‘EMULATION_STATE’ and is stuck in the ‘SENSE_STATE’ of the implemented NFCTarget_statemachine function. This is happening because every time the NFC_TARGET_PROTOCOL register is read after an RF field is detected by EVM it returns a 0xC0 value meaning that it is unable to recognize the initiator command at all and only detects an RF wakeup.
Please help diagnose the problem or suggest a different example code. Thanks a lot.
Best Regards
Hammad