I'm using the CC1000 at 425 MHz in an application where it is sharing an antenna (through a passive diplexer network with a GSM radio operating in the 900 MHz and 1800 MHz bands. I need to know the maximum RF power in these bands that can be present on the 'RF_IN' pin without DAMAGE to the CC1000. I'd also like to know the maximum power in these bands above which PERFORMANCE of the CC1000 will be adversely affected (operating at 425 MHz).
In the 'Absolute Maximum Ratings' section of the CC1000 datasheet, the maximum input RF level is given as +10 dBm, but I assume this is an IN-BAND spec (whereas I'm interested in maximum OUT-OF-BAND power). The only thing I see related to out-of-band rejection is a 'blocking' spec in the 'Receive Section' portion of Table 3: "blocking = 40 dBc @ +/- 1 MHz", but this says nothing about the rejection at frequencies that are much further out.
Thank you.