Hi,
Please tell me about ADC differential input(CC2543).
*Question
I want to input Audio signal using a function of differential input.
By the setting of this register and the connection method of the plug, will Differential-input function?
I feel that differential-input does not function even if I perform this setting in my environment.
Please tell me the mistake ている point.
*development environment:
SmartRF05 Evaluation Board Rev.1.8.1
CC2543
Mic Input Balanced(Hot,Cold,GND)
*Setting of ADC Registers:
ADCCON2
SREF 11: External reference on AIN6-AIN7 differential input
SDIV 10: 256 decimation rate (10 bits ENOB setting)
SCH 1011: AIN6-AIN7
*Plug connection:
Audio signal CC2543
Hot Plug --> AIN6
Cold Plug --> AIN7
GND Plug --> GND