I have connected 2 SmartRf05EB board with CCMSP-EM430F2618 to which I connected CC2520DK-EM and loaded example PER-Test program into it Using CODE COMPOSER STUDIO..and acheived the correct result..
Now i want to do the same using SMARTRF STUDIO7 hwere we need to remove "CCMSP-EM430F2618" and directly attach CC2520 to SmartRf05EB and the RF is being detected in SmartRf Studio7..and I opted for Easy Mode and set the required fields like Tx power n Frequency according to that done when I did with the "CCMSP-EM430F2618" connected..and start the transmission and reception there is result cmng perfectly..i.e. if i gve 100 packets im getting that count..or in export mode if i send hex value im getting the same at receiver..
bt d pblm is whn i changed even the frequency n tx power whch is not according to the setting i made when "CCMSP-EM430F2618" is connected to SmartRf05EB..finally it is nt working according to the required..
How can i come across?? Can i Program according to my requiremnt and control CC2520 accordingly