Hi,
I'm having trouble with the msp430f5529lp board and the DLP7970A booster pack.
I have downloaded and installed the NFC player, installed uniflash and followed the instructions documented here
http://www.ti.com/lit/ml/slab069/slab069.pdf
However the heartbeat LED never flashes.
I have seen several posts that have similar issues such as this one http://e2e.ti.com/support/wireless_connectivity/f/667/t/332903.aspx
I have also downloaded and tried programming different .out files such as eh one suggested here http://e2e.ti.com/support/wireless_connectivity/f/667/p/298945/1042210.aspx#1042210
but no matter what I do I cannot get the LED to flash and I get the following in eth nfc player log file
23:47:39:901 CNfcPlayer::nfcStart: Enter
23:47:39:901 CNfcPlayer::nfcStart: Global NFC flags: 0xF2FF39F7, L1 flags: 0x03050030 - will be ignored if local (configuration-specific) flags are set
23:47:39:901 CNfcPlayer::nfcStart: No local TRACES.NFC parameter found - adding global or default parameter
23:47:39:901 CNfcPlayer::nfcStart: No local TRACES.L1 parameter found - adding global or default parameter
23:47:39:901 CNfcPlayer::nfcStart: Initialization <READERTYPE=TRF7970 IOTYPE=SERIAL PORT=COM13 TRACES.NFC=f2ff39f7 TRACES.L1=03050030>
23:47:39:901 CNfcInstance::nfcStart: Enter
23:47:39:901 CNfcInstance::nfcStart: NFC library loaded
23:47:39:901 CNfcInstance::nfcStart: NFC API version: 2.3
23:47:39:901 CNfcInstance::nfcStart: NFC stack version: 2.2.0.4
23:47:39:916 CNfcInstance::nfcStart: NFC controller initialized
23:47:41:938 ! CNfcInstance::nfcStart: Creating a RW-NFC-instance failed (code: 4)
23:47:41:938 ! CNfcPlayer::nfcStart: Instance initialization failed (code: 4)
I cannot compile the RW_P2P_CE_1 project hence looking for a good .out file
My customer as the same hardware as I do and he is getting the exact same errors - please help.
Cheers
Calum