This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sub 1 Ghz daugter boards for MSP430 EVM

Other Parts Discussed in Thread: CC1101, CC2530EM

Hello,

The EVM430-F6779 - 3 Phase Electronic Watt-Hour EVM for Metering mentions that there are:

"Add-on communications modules for wireless communications standards such as ZigBee ®, Wi-Fi®, Wireless M-Bus, and IEEE-802.15.4g. Both 2.4GHz and Sub-1GHz."

Do you know which boards can connect to this EVM? I am looking for specifically a 6LoWPAN sub 1 Ghz board.

I have also seen this module: http://www.anaren.com/air/products/915mhz-solutions

Can these modules connect to the EVM?

I would appreciate your help with this matter.

Regards,

David

  • David, 

    I have not been able to find the schematic for the EVM430-F6779 to verify but it is the intention with the EM connector interface that most of our development kits and also our module vendors developments kits will plug in without issues.

    I have only seen the Zigbee (CC2530EM) uses with this development kit, but I know that the connector interface is compatible with our CC1101 EM board.

    I would say yes, but I cannot confirm it.

    Regards,
    /TA

  • Thank you for your help. I will look into this more, but I think this will work.

    Thanks again,

    David