Dear TI,
I'm struggling for days now to get the asynchronous serial mode working. For some reason i dont receive anything on my 433.92 Mhz receiver.
This i've tested right now:
- settings the CC1101 config and read it back to make sure the config in the cc1101 is set
- testing if there is a signal on the gdo0 pin
- Testing SPI communication with logic analyzer. (i've received data anyway)
- Tested the receiver with a 433.92Mhz remote controller
this is the driver im using:
The main code:
static struct sCC1101 gCC1101Settings = {
0x0B, // IOCFG2 GDO2 Output Pin Configuration
0x2E, // IOCFG1 GDO1 Output Pin Configuration
0x2E, // IOCFG0 GDO0 Output Pin Configuration
0x47, // FIFOTHR RX FIFO and TX FIFO Thresholds
0xD3, // SYNC1 Sync Word, High Byte
0x91, // SYNC0 Sync Word, Low Byte
0xFF, // PKTLEN Packet Length
0x04, // PKTCTRL1 Packet Automation Control
0x32, // PKTCTRL0 Packet Automation Control
0x00, // ADDR Device Address
0x00, // CHANNR Channel Number
0x06, // FSCTRL1 Frequency Synthesizer Control
0x00, // FSCTRL0 Frequency Synthesizer Control
0x10, // FREQ2 Frequency Control Word, High Byte
0xB1, // FREQ1 Frequency Control Word, Middle Byte
0x21, // FREQ0 Frequency Control Word, Low Byte
0xC7, // MDMCFG4 Modem Configuration
0x02, // MDMCFG3 Modem Configuration
0x30, // MDMCFG2 Modem Configuration
0x00, // MDMCFG1 Modem Configuration
0x7A, // MDMCFG0 Modem Configuration
0x15, // DEVIATN Modem Deviation Setting
0x07, // MCSM2 Main Radio Control State Machine Configuration
0x30, // MCSM1 Main Radio Control State Machine Configuration
0x18, // MCSM0 Main Radio Control State Machine Configuration
0x14, // FOCCFG Frequency Offset Compensation Configuration
0x6C, // BSCFG Bit Synchronization Configuration
0x03, // AGCCTRL2 AGC Control
0x40, // AGCCTRL1 AGC Control
0x91, // AGCCTRL0 AGC Control
0x87, // WOREVT1 High Byte Event0 Timeout
0x6B, // WOREVT0 Low Byte Event0 Timeout
0xFB, // WORCTRL Wake On Radio Control
0x56, // FREND1 Front End RX Configuration
0x11, // FREND0 Front End TX Configuration
0xE9, // FSCAL3 Frequency Synthesizer Calibration
0x2A, // FSCAL2 Frequency Synthesizer Calibration
0x00, // FSCAL1 Frequency Synthesizer Calibration
0x1F, // FSCAL0 Frequency Synthesizer Calibration
0x41, // RCCTRL1 RC Oscillator Configuration
0x00, // RCCTRL0 RC Oscillator Configuration
0x59, // FSTEST Frequency Synthesizer Calibration Control
0x7F, // PTEST Production Test
0x3F, // AGCTEST AGC Test
0x81, // TEST2 Various Test Settings
0x35, // TEST1 Various Test Settings
};
struct sCC1101PhyInfo gPhyInfo;
struct sCC1101Spi gSpi = { SpiInit, SpiRead, SpiWrite };
uint8_t gPaTable[8] = { 0x60, 0xC0, 0xC0, 0xC0, 0xC0, 0xC0, 0xC0, 0xC0 };
int main(void) {
// mcu init
sysclk_init();
board_init();
udc_start();
kk_init();
// cc1101 init
CC1101SpiInit(&gPhyInfo, &gSpi, NULL);
//CC1101Reset(&gPhyInfo);
CC1101WriteRegisters(&gPhyInfo, CC1101_PATABLE, gPaTable, 8);
CC1101Configure(&gPhyInfo, &gCC1101Settings );
CC1101Transmit(&gPhyInfo);
kaku_send(13,14,1,0); // send a signal to GDO0
Please help me to fix t his, because it really drives me crazy.