This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello members
I did a P2P test on two EVM. but it does not work.
GUI will get an error dialog.
error message is [Set New Target CID number]
Why does not work, I want you to tell me the cause
Condition
use evm:TRF7970AEVM
PC:windows 7 64bit OS
GUI:TRF7970AEVM GUI WIN 7(11/13/2013)
FirmWare Version:03_08_2013
[Initiator Log]
10:32:34.459 COM12
10:32:34.459 COM11
10:32:34.459 COM10
10:32:34.459 COM9
10:32:34.459 COM8
10:32:34.475 --> 0108000304FF0000
10:32:34.506 <-- TRF7970A EVM
10:32:34.506 **** COM Port found! ****
10:33:40.290 --> 00F
10:33:40.290 COM8
10:33:40.727 <-- 0
10:33:40.727 --> 010C00030410002101310000
10:33:41.257 <-- Register write request.
10:33:41.257 portSetReadMode
10:33:41.257 --> 010B000304D403D4F00000
10:33:41.397 <-- NFC.[00]
10:33:48.854 --> 0109000304A0010000
10:33:49.057 <-- 14443A REQA.
10:33:49.057 --> 0109000304A0010000
10:33:49.244 <-- 14443A REQA.
10:33:49.244 --> 0109000304A0010000
10:33:49.431 <-- 14443A REQA.
10:33:49.431 --> 0109000304A0010000
10:33:49.618 <-- 14443A REQA.
10:33:49.618 --> 0109000304A0010000
10:33:49.806 <-- 14443A REQA.
10:33:54.875 Set new target CID number
[Target Log]
10:20:00.749 COM12
10:20:00.765 COM11
10:20:00.765 COM10
10:20:00.765 COM9
10:20:00.890 --> 0108000304FF0000
10:20:00.936 <-- []TRF7970A EVM
10:20:00.936 **** COM Port found! ****
10:20:18.663 --> 00F
10:20:18.663 COM9
10:20:19.240 <-- 0
10:20:19.240 --> 010C00030410002101210000
10:20:19.770 <-- Register write request.
10:20:19.770 --> 0115000304D40DD40C0123456789ABCDEF01230000
10:20:20.207 <-- NFC.
hi
We've done some test but, peer to peer mode of TRF7970A EVM does not work.
I have compared the TI-GUI and UsersGuide, I found some of the differences.
ISO14443A of GUI Tab
Part of the red frame is different from the user guide page 27 of (SLOU321) Figure22.
Is this not a problem?
TI-GUI ISO14443B Tab
(SLOU321 Figure24 of 31 pages of parts and user guide of red frame There is a difference.
Is this not a problem?
TEST Tab
1)
I sent the command of user guide (SLOU321) of 43 page Table8 to EVM.
but, LED is not toggle action.
2)
Not be echoed back.
I was sent in accordance with user guide (SLOU321), but are not echo back.
Thank you for the answer.
I understand that it will not be updated even if there is trouble in the future.
In the future I will evaluate in the MSP430F5529 EVM or LaunchPad.
Thank you.
Dear Alexander Kozitsky,
i am using the same 2 EVM modules for my thesis project i want to demonstrate p2p functionality one as target and other as initiator but when i try to to push connect button i get mentioned below errors.
i am using windows 7 64x and all proper USB drivers are installed i am stuck here please help of suggest something in to order to get rid of this problem.
Thanking you and kind regards
Muhammad Haris
14:43:57.407 COM12
14:43:57.409 COM11
14:43:57.410 COM10
14:43:57.411 COM9
14:43:57.412 COM8
14:43:57.412 COM7
14:43:57.413 COM6
14:43:57.413 COM5
14:43:57.414 COM4
14:43:57.414 COM3
14:43:57.504 --> 0108000304FF0000
14:43:57.553 <-- TRF7970A EVM
14:43:57.555 **** COM Port found! ****
14:44:06.722 --> 00F
14:44:06.732 COM3
14:44:07.157 <-- 0
14:44:07.166 --> 010C00030410002101310000
14:44:07.683 <-- Register write request.
14:44:07.692 portSetReadMode
14:44:07.701 --> 010B000304D403D4F00000
14:44:07.818 <-- NFC.[00]
14:44:10.571 --> 0109000304A0010000
14:44:10.749 <-- 14443A REQA.
14:44:10.758 --> 0109000304A0010000
14:44:10.936 <-- 14443A REQA.
14:44:10.941 --> 0109000304A0010000
14:44:11.114 <-- 14443A REQA.
14:44:11.123 --> 0109000304A0010000
14:44:11.301 <-- 14443A REQA.
14:44:11.310 --> 0109000304A0010000
14:44:11.489 <-- 14443A REQA.
14:44:15.308 Set new target CID number