Dear All,
I found the post on the website(
e2e.ti.com/.../231315) that is relevant to my problem.
I would like to add a RF switch(PE4259, www.psemi.com/.../pe4259) on the pin1 of a balun (2450BM15A0002, www.ti.com/.../swra297b.pdf) of CC2540. As I am new to impedance matching and EM simulation, I do not know whether I need to add the matching network between the pin1 of balun and the extra RF switch? and between RF switch to chip antenna(www.johansontechnology.com/.../2450AT42A100_v2.pdf)? and how to make it ? Is there any reference design regarding adding RF switch with keeping the same Tx and Rx power efficiency?
I find the note in the post and think it is a good start to learn from scratch. First, I try to do ADS simulation on the first part of the note about differential matching network. As I do not how to fill MLIN microstrip model (W or L), I short it. I keep default values of Q= 50, Rdc=0 Ohm for INDQ and default values of R=1 Ohm, L=1nH for SRLC. The S11 (on the match common point of C252 and L261) of -18 dB occurs by 2.8nH and 0.8pF rather than 2.2nH and 0.8pF in the post. How do I correct my simulation result to meet the results in the post ?
Best Regards,
TS