Hello Team,
I'm working on an RFID multiplexer design using the SLOA167 application note. The application note says there is code available in a separate zip file (TRF7960A_MUX.zip). I wasn't able to find this code when I searched for it. Can someone please provide me with this code? Also, if there is a version for the TRF7970A, could you provide that as well or explain what changes may need to be made to the '60A code?