I'm designing a system with the CC1020 using SmartRF studio (thanks your to previous help, also).
I'm trying to understand how what happens if the frequency separation of a 2-FSK system is lower than the baudrate.
I found that this frequency should be, for narrow band systems, ideally the same as the baudrate. Could be greater than this, and I'm obtaining a wide band system. That's ok.
My question is what happens if the separation is lower than the baudrate? I'm asking this because the CC1020 transceiver, with high baudrate (153600), with a frequency separation of more than 153kHz, will not obtain a proper configuration with its SmartRF studio configuration. The option is to reduce the crystal uncertainty or the frequency separation, while the channel spacing is already set to maximum (500kHz).
My system is half duplex, with same frequency in RX and TX (work alternatively on the same chip). At this moment, if too much wideband, could be still ok.
Thanks to all.