This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RemoTI Unicast/NoAck/SC

Other Parts Discussed in Thread: REMOTI

Hi

In the RemoTI Developer's Guide there is a discussion of the Transmission Options available; one of them being the Unicast/NoAck/SC that I would like to use to increase data throughput. It explains that this option can be configured in the RTI_SendDataReq() function for the controller.

How does one do this on the Target too?

In other words, after pairing, when both the Controller and the Target have decided on the channel, I would like to transmit and make sure that the Target is listening on the original channel.

Thank you


Best regards