Hi guys,
Can you tell me how the thickness of PCB depends on NFC antenna design? Are there any constraints for PCB design? If so how i can overcome such issues?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi guys,
Can you tell me how the thickness of PCB depends on NFC antenna design? Are there any constraints for PCB design? If so how i can overcome such issues?
Hi Riyaz,
PCB thickness and copper weight will affect the inductance of the antenna coil, especially when you are using two sides of the PCB for the coil. If the coil is only using one side of the PCB, the PCB thickness should not affect it, but a difference in copper weight would. Heavier copper will provide a lower inductance. Typical FR4 uses 1.5oz copper weight and flex PCB typical is 0.5oz copper. On an FR4 PCB with 6 turns(3 on top, 3 on bottom), I see about 2uH. With the exact same layout manufactured on flex PCB, I see about 4.2uH. This additional inductance is mostly due to the reduced spacing between the top and bottom layer coils on flex PCB.
Can you provide additional details about your PCB and antenna design? I can help make some specific suggestions with more detail. Thanks!